CMPx.SOURCEVALUE
Description
Reads the current value of the selected source for CMPx.SOURCE.
Example
If CMP0.SOURCE = 3 (PL.FB), CMP0.SOURCEVALUE will return the current value of PL.FB.
General Information
|
Type |
R/O Parameter |
|
Units |
Units depend on value of CMPx.SOURCE. See table below. |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Start Version |
M_01-13-00-000 |
Units
| CMPx.SOURCE | Units |
|---|---|
| 0 (FB1) | Depends on FB1.PUNIT or custom units. |
| 1 (FB2) | Depends on FB2.PUNIT or custom units. |
| 2 (FB3) | Depends on FB2.PUNIT or custom units. |
| 3 (PL.FB) | Depends on UNIT.PLINEAR
or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts Linear: counts, mm, µm, (custom units), 16-bit counts |
Hardware Supported
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC | Revision DA or higher |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | See SynqNet Supported Parameters |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | No |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
| Paramter |
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|---|
| CMP0.SOURCEVALUE |
Profinet |
2961 |
DWord | Yes |
| sercos® III | 8 Octets | |||
| CMP1.SOURCEVALUE |
Profinet |
2963 | DWord | |
| sercos® III | 8 Octets |
| Fieldbus | Parameter | Instance | Data Size | Data Type |
|---|---|---|---|---|
| EtherNet/IP | CMP0.SOURCEVALUE | 962 | 8 Byte Signed | Float |
| CMP1.SOURCEVALUE | 964 |
Related Topics