CMPx.WIDTHTYPE
Description
Use this keyword to set the width-type for a Compare setpoint. The width-type determines whether the width of the Compare pulse is in position counts or units of time (microseconds).
Example
The following example sets the width type of setpoint 7 to microseconds, and the width of setpoint 7 to 1000 microseconds.
-->CMP0.WIDTHTYPE 7 1
-->CMP0.WIDTH 7 1000
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 (position) to 1 (time) |
|
Default Value |
0 |
|
Data Type |
Argument 1:Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Hardware Supported
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC | Revision DA or higher |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | No |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
| Fieldbus | Index/Subindex | Object Start Version | |
|---|---|---|---|
|
EtherCAT COE and CANopen |
34ACh/1 | CMP0.WIDTHTYPE 0 | M_01-13-00-000 |
| 34AAh/2 | CMP0.WIDTHTYPE 1 | ||
| 34AAh/3 | CMP0.WIDTHTYPE 2 | ||
| 34AAh/4 | CMP0.WIDTHTYPE 3 | ||
| 34AAh/5 | CMP0.WIDTHTYPE 4 | ||
| 34AAh/6 | CMP0.WIDTHTYPE 5 | ||
| 34AAh/7 | CMP0.WIDTHTYPE 6 | ||
| 34AAh/8 | CMP0.WIDTHTYPE 7 | ||
|
34BCh/1 |
CMP1.WIDTHTYPE 0 | ||
|
34BAh/2 |
CMP1.WIDTHTYPE 1 | ||
|
34BAh/3 |
CMP1.WIDTHTYPE 2 | ||
|
34BAh/4 |
CMP1.WIDTHTYPE 3 | ||
|
34BAh/5 |
CMP1.WIDTHTYPE 4 | ||
|
34BAh/6 |
CMP1.WIDTHTYPE 5 | ||
|
34BAh/7 |
CMP1.WIDTHTYPE 6 | ||
|
34BAh/8 |
CMP1.WIDTHTYPE 7 | ||
| Paramter |
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|---|
| CMP0.WIDTHTYPE |
Profinet |
2922 |
Byte | No |
| sercos® III | 2 Octets | |||
| CMP1.WIDTHTYPE |
Profinet |
2929 | Byte | |
| sercos® III | 2 Octets |
| Fieldbus | Parameter | Instance | Data Size | Data Type |
|---|---|---|---|---|
| EtherNet/IP | CMP0.WIDTHTYPE | 923 | 1 Byte | Integer |
| CMP1.WIDTHTYPE | 930 |
Related Topics