COGCOMP.SAVE

Description

This parameter saves the current cogging compensation table (COGCOMP.CORRECTIONTABLE) from RAM to NV memory. On next drive boot, the cogging compensation table will be initialized with the stored entries from NV.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-14-07-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

3038

Word No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 1039 2 Byte None

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed? Object Start Version

Modbus

2892

No Command No M_01-14-07-000