CPS.ACTIVE

Description

CPS.ACTIVE reads the enable status of the AKD-C:

 Value Description
0 No system power (inrush opened).
1 Strings not fully powered (inrush closed). AKD-Ns cannot be enabled. The AKD-C has a fault which disables the AKD-Ns and unpowers the strings.
3

Strings powered and drives disabled. AKD-Ns cannot be enabled. The AKD-C has a fault which only disables the AKD-N's control board temperature.

7 Strings powered and drive operational. All AKD-Ns can be enabled. The AKD-C has no faults and strings are fully powered.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-04-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes