DRV.CUSTOMIDENTIFIER

Description

Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:

  • ASCII characters only
  • 32 character max length
  • No spaces in string

The string is displayed on the device overview screen and in the start page's device discovery table.

General Information

Type

NV Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-12-05-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

2032h/0

M_01-12-05-000

Related Topics

DRV.NAME