DRV.SETUPREQBITS

Description

This parameter returns the bitwise set status of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.


  • If MOTOR.AUTOSET is set to 1 (parameters automatically calculated from motor ID data), then all values in the list will be initialized from the feedback device. Otherwise, the parameters must be set manually.

The following table lists the parameters which require setup for each motor type.

Parameter Bit Default Value Linear Permanent Magnet Induction Motor V/f Open Loop Induction Motor Closed Loop Interior Permanent Magnet Brush Motor
IL.KP 0 50 [V/A] -
MOTOR.IPEAK 1 2 Arms
MOTOR.ICONT 2 1 Arms
MOTOR.POLES 4 6 -
MOTOR.LQLL 7 17mH - - - -
MOTOR.LDLL 8 17mH - - - -
MOTOR.KE 9 0 - - - -
MOTOR.IMTR 10 100ms - - - -
MOTOR.IMID 11 0 - - - -
MOTOR.VOLTRATED 12 230 Vrms - - - -
MOTOR.VRATED 13 0 - - - -
MOTOR.LISAT 14 25 x DRIVE.IPEAK - - - -
MOTOR.VRIDK1 15 0 - - - -
MOTOR.VRIDK2 16 0 - - - -
MOTOR.IDMAX 17 0.5 x MOTOR.IPEAK - - - -
IL.KDPRATIO 18 1 - - - -
MOTOR.PITCH 19 32 - - - -
MOTOR.VOLTMAX 20 480 Vrms - - -

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2805

DWord Yes
sercos® III 8 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 791 4 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1580

No 32-bits No

M_01-06-03-000

Related Topics

DRV.SETUPREQLIST, MOTOR.AUTOSET