DRV.STOP

Description

This command stops drive motion. In torque and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.

If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.

The following table defines the behavior of DRV.STOP:

Cmdsource Opmode Subopmode Deceleration ramp defined by:
Service Torque - IL.CMD = 0
Velocity - If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used.
Position Service motion If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used.
Motion tasking MT.DEC
Homing HOME.DEC
Fieldbus Torque - Command has no effect.
Velocity
Position
Electronic Gearing Position - GEAR.DECMAX
Analog Torque - Command has no effect.
Velocity
Position

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

35FEh/0

M_01-00-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2137

Command* No
sercos® III

*For Profinet, write a value of 0 into the PNU to execute a command.

Fieldbus Instance Data Size Data Type
EtherNet/IP 138 Command None

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

274

No Command No

M_01-03-00-000