DRV.TYPE

Description

DRV.TYPE allows you to select the operational fieldbus for your drive. This parameter is read-write on the CC drive models and read-only on all other drive models. To change the operational fieldbus of your drive:

  1. Set DRV.TYPE to one of the following values. Only values 0 to 3 are selectable. All other values are read only.

    0 = Analog (no EtherCAT or CANopen) with no position indexer functionality.
    1 = Analog (no EtherCAT or CANopen) with position indexer functionality.
    2 = EtherCAT
    3 = CANopen
    4 = SynqNet
    5 = EtherNet/IP
    6 = BASIC Langauge (not fieldbus)
    7 = Profinet
    8 = sercos® III
  1. Save the parameters to the NV memory on the drive by issuing the DRV.NVSAVE command
  2. Power cycle the 24 V supply to the drive. When the drive has finished powering up, it will be working with the new selection.

Changing DRV.TYPE does not immediately change the type of the drive fieldbus selection. You must power cycle the drive to start the drive with the selected functionality.

You cannot use EtherCAT and CANopen at the same time. Use FBUS.TYPE or DRV.INFO to identify the fieldbus currently in use.

DRV.TYPE does not change if you use DRV.RSTVAR.

General Information

Type

R/W on the CC drive model. R/O on all other drive models.

Units

N/A

Range

0 to 8

Default Value

2

Data Type

Integer

Start Version

M_01-03-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2138

Byte No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 139 1 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

276

No 8 bit No

M_01-03-00-000

Related Topics

AKD Modelle

FBUS.TYPE, DRV.INFO