ECAT.ENEMCYREQ
Description
This parameter is used to enable or disable the EtherCAT emergency messaging.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-18-03-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | Yes |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No* |
| AKD EtherNet/IP | No |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.