FAULTx.ACTION

Description

This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.

Parameter Value Drive Action
0 Disable Ampllifier
1 Ignore (fault will not be reported)

General Information

Type

R/W

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-04-16-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

5259h /0 FAULT130.ACTION M_01-04-16-000
525Ah /0 FAULT131.ACTION
525Bh /0 FAULT132.ACTION
525Ch /0 FAULT134.ACTION

5267h /0

FAULT451.ACTION
525Dh /0 FAULT702.ACTION

Parameter

Fieldbus

Address

Attributes Signed?
FAULT130.ACTION

Profinet

2601

Byte No
sercos® III 2 Octets
FAULT132.ACTION

Profinet

2602 Byte
sercos® III 2 Octets
FAULT130.ACTION

Profinet

2603 Byte
sercos® III 2 Octets
FAULT132.ACTION

Profinet

2604 Byte
sercos® III 2 Octets
FAULT139.ACTION

Profinet

2797 Byte
sercos® III 2 Octets
FAULT451.ACTION

Profinet

2615 Byte
sercos® III 2 Octets
FAULT702.ACTION

Profinet

2605 Byte
sercos® III 2 Octets

Fieldbus

Parameter

Instance

Data Size Data Type
EtherNet/IP FAULT130.ACTION 602 1 Byte Integer
FAULT131.ACTION 603
FAULT132.ACTION 604
FAULT134.ACTION 605
FAULT139.ACTION 798
FAULT451.ACTION 616
FAULT702.ACTION 606

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?
Modbus 1202 FAULT130.ACTION No 8 bit

No

1204 FAULT131.ACTION
1206 FAULT132.ACTION
1208 FAULT134.ACTION
1594 FAULT139.ACTION
1210 FAULT702.ACTION
1230 FAULT451.ACTION