FBUS.PARAM1 TO FBUS.PARAM10

Description

FBUS.PARAM01 sets the baud rate for the CANbus. Supported baud rates are 125, 250, 500 and 1000 kBaud on AKD-C

FBUS.PARAM01 sets and stores the EtherCAT station alias for the ESC (EtherCAT slave controller) of string 2.

FBUS.PARAM02 switches the phase locked loop (PLL) for synchronized use: 0 = OFF, 1 = ON. FBUS.PARAM02 only works when FBUS.TYPE = 3 (CANopen).

FBUS.PARAM03 sets and stores the EtherCAT station alias for the ESC (EtherCAT slave controller). On AKD-C, FBUS.PARAM03 sets and stores the EtherCAT station alias for the ESC (EtherCAT slave controller) of string 1.

FBUS.PARAM04 switches the surveillance of SYNC-signals: 0 = OFF, 1 = ON.

FBUS.PARAM05 is used to configure some special behaviors of the DS402.

FBUS.PARAM06 - FBUS.PARAM10 are reserved.

 

FBUS.PARAM04 Additional Notes

FBUS.PARAM04 enables (1) or disables (0) the synchronization supervision of the CANopen or EtherCAT fieldbus.

Default values for this parameter:

  • CANopen drive: disabled (0)
  • EtherCAT drive: enabled (1)

Synchronization supervision is active when FBUS.PARAM 04 = 1 and the first CANOpen Sync message or first EtherCAT frame is received. When more than three CANopen sync messages or seven EtherCAT frames have not been received and the drive is enabled, fault F125 (“Synchronization lost“) occurs.

FBUS.PARAM05 Additional Notes

Bit 0 configures the behavior of DS402 state machine in case of fault resets.

(missing or bad snippet)

General Information

Type

NV Parameter

Units

N/A

Range

See table below.

Default Value

See table below.

Data Type

Unsigned 32

See Also

CANbus Communication Manual, EtherCAT Communication Manual

Start Version

M_01-00-00-000

ParameterEtherCAT COE RangeCANopen Range
FBUS.PARAM01

AKD-C: 0 to 65,535

Other AKDs: N/A

125; 250; 500; 1000
FBUS.PARAM020 to 10 to 1
FBUS.PARAM030 to 65,535N/A
FBUS.PARAM040 to 10 to 1
FBUS.PARAM050 to 5110 to 511
ParameterEtherCAT COE Default ValueCANopen Default Value
FBUS.PARAM01

AKD-C: 0

Other AKDs: N/A

125

FBUS.PARAM02

1

0

FBUS.PARAM03

0

N/A

FBUS.PARAM04

1

0

FBUS.PARAM05

0

0

Variants Supported

VariantSupported
AKD BaseYes
AKD with Position IndexerYes
AKD EtherCATYes
AKD CANopenYes
AKD BASICNo
AKD SynqNetYes*
AKD EtherNet/IPYes
AKD ProfinetYes
AKD sercos® IIIYes
AKD-NYes
AKD-CYes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

FieldbusIndex/SubindexObject Start Version

EtherCAT COE and CANopen

36E5h/0

FBUS.PARAM01

36EAh/0

FBUS.PARAM06

M_01-00-00-000

36E6h/0

FBUS.PARAM02

36EBh/0

FBUS.PARAM07

36E7h/0

FBUS.PARAM03

36ECh/0

FBUS.PARAM08

36E8h/0

FBUS.PARAM04

36EDh/0

FBUS.PARAM09

36E9h/0

FBUS.PARAM05

36EEh/0

FBUS.PARAM10

Paramter

Fieldbus

Address

AttributesSigned?
FBUS.PARAM1

Profinet

2157DWordNo
sercos® III4 Octets
FBUS.PARAM2

Profinet

2158DWord
sercos® III4 Octets
FBUS.PARAM3

Profinet

2159DWord
sercos® III4 Octets
FBUS.PARAM4

Profinet

2160DWord
sercos® III4 Octets
FBUS.PARAM5

Profinet

2161DWord
sercos® III4 Octets
FBUS.PARAM6

Profinet

2162DWord
sercos® III4 Octets
FBUS.PARAM7

Profinet

2163DWord
sercos® III4 Octets

Fieldbus

ParameterInstanceData SizeData Type
EtherNet/IPFBUS.PARAM011584 byteInteger
FBUS.PARAM02159
FBUS.PARAM03160
FBUS.PARAM04161
FBUS.PARAM05162
FBUS.PARAM06163
FBUS.PARAM07164

Fieldbus

 

Index/Subindex

Is 64 bit?AttributesSigned?

Object Start Version

ModbusFBUS.PARAM01314No32 bitNoM_01-03-00-000
FBUS.PARAM02316
FBUS.PARAM03318
FBUS.PARAM04320
FBUS.PARAM05322
FBUS.PARAM06324
FBUS.PARAM07326
FBUS.PARAM08328
FBUS.PARAM09330
FBUS.PARAM10332