IL.FOLDFTHRESH

Description

IL.FOLDFTHRESH is the fault level of the current foldback algorithm. If IL.IFOLD drops below the value for IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.

To avoid reaching the current foldback fault level, set IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the IL.FOLDFTHRESHU value to zero.

General Information

Type

R/O Parameter

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (DRV.IPEAK)

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

3420h/0

M_01-00-00-000

Fieldbus

Address

Attributes Signed?

Profinet

2218

DWord No
sercos® III 4 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 219 4 Byte Float

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

436

No 32 bit No

M_01-03-00-000

Related Topics

Current Loop