IL.KPLOOKUPINDEX
Description
This parameter sets the index into the Current Loop Gain Scheduling Table. The table is 256 records long, spanning 0 A to 1.62 * DRV.IPEAK.
To determine the level of current that corresponds to a table index, use the following equation:
IL.CMD = (Table Index /157) * DRV.IPEAK
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 to 255 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-04-00-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Index/Subindex |
Object Start Version |
|---|---|---|
|
EtherCAT COE and CANopen |
5265h /0 |
M_01-04-00-000 |
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
2613 |
Word | No |
| sercos® III | 2 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 614 | 2 Byte | Integer |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
|---|---|---|---|---|
| Modbus | 1226 | No | 16 bit |
No |
Related Topics
Current Loop