IL.KPSOURCE
Description
Sets the source of the IL.KP value when MOTOR.AUTOSET is enabled.
| 0 | The Autoset feature calculates IL.KP from motor parameters |
| 1 | IL.KP is read from NV (or set to the default value if no value is stored) |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-14-06-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | Yes |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
|
Fieldbus |
Address |
Attributes | Signed? |
|---|---|---|---|
|
Profinet |
3034 |
Byte | No |
| sercos® III | 2 Octets |
| Fieldbus | Instance | Data Size | Data Type |
|---|---|---|---|
| EtherNet/IP | 1035 | 1 Byte | Integer |
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
2884 |
No | 8 bit | No |
M_01-14-06-000 |