IP.EOEADDRESS

Description

IP.EOEADDRESS displays the EoE IP address. If no EtherCat Master with EoE is connected, the return value is 0.0.0.0.

General Information

Type

R/O Parameter

Description Displays the EoE IP address

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-18-01-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen No
AKD Basic No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N Yes
AKD-C Yes
AKD-N Yes
AKD-C Yes