IP.EOEMACADDRESS
Description
IP.EOEMACADDRESS displays the EoE Mac address. If no EtherCat Master with EoE is connected, the return value is 00-00-00-00-00-00.
General Information
|
Type |
R/O Parameter |
| Description | Displays the EoE mac address |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-18-01-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | Yes |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No |
| AKD EtherNet/IP | No |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | Yes |
| AKD-C | Yes |
| AKD-N | Yes |
| AKD-C | Yes |