JOG.DEC
Description
This parameter sets the deceleration ramp for jog moves.
General Information
|
Type |
NV Parameter |
|
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR |
|
Range |
0.224 to 240000008.192 rpm/s |
|
Default Value |
10000.000 rpm/s |
|
Data Type |
Float |
|
Start Version |
M_01-19-06-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | Yes |
| AKD with Position Indexer | Yes |
| AKD EtherCAT | Yes |
| AKD CANopen | Yes |
| AKD BASIC | No |
| AKD SynqNet | Yes* |
| AKD EtherNet/IP | Yes |
| AKD Profinet | Yes |
| AKD sercos® III | Yes |
| AKD-N | Yes |
| AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.