MODBUS.ERRORMODE

Description

Enables or disables error response messages.

Value Description
0 Send error response messages (default).
1 Do not send error response messages.

General Information

Type

R/W

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-08-03-001

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet No
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Address Attributes Signed?
sercos® III 2878 2 Octets No
Fieldbus Instance Data Size Data Type
EtherNet/IP 879 1 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

1756

No 8 bit No

Related Topics

MODBUS.CLRERRORS | MODBUS.ERRORS