PLS.T1 TO PLS.T8

Description

These parameters define the time of the PLS pulse for time-based PLS handling.

For further information about the PLS functionality, especially the meaning of the PLS.T1 to PLS.T8 parameter, refer to the PLS.UNITS parameter.

General Information

Type

R/W parameter

Units

ms

Range

0 to 65,536 ms

Default Value

500 ms

Data Type

Integer

See Also

PLS.EN, PLS.RESET, PLS.STATE, PLS.UNITS, PLS.MODE, PLS.WIDTH1 TO PLS.WIDTH8, PLS.P1 TO PLS.P8

Start Version

M_01-02-03-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus Index/Subindex Object Start Version

EtherCAT COE and CANopen

34A2h/1

PLS.T1

M_01-02-03-000

34A2h/2

PLS.T2

34A2h/3

PLS.T3

34A2h/4

PLS.T4

34A2h/5

PLS.T5

34A2h/6

PLS.T6

34A2h/7

PLS.T7

34A2h/8

PLS.T8

Paramter

Fieldbus

Address

Attributes Signed?
PLS.T1

Profinet

2329 Word No
sercos® III 2 Octets
PLS.T2

Profinet

2330 Word
sercos® III 2 Octets
PLS.T3

Profinet

2331 Word
sercos® III 2 Octets
PLS.T4

Profinet

2332 Word
sercos® III 2 Octets
PLS.T5

Profinet

2333 Word
sercos® III 2 Octets
PLS.T6

Profinet

2334 Word
sercos® III 2 Octets
PLS.T7

Profinet

2335 Word
sercos® III 2 Octets
PLS.T8

Profinet

2336 Word
sercos® III 2 Octets

Fieldbus

Parameter

Instance

Data Size Data Type

EtherNet/IP

PLS.T1

330 2 Byte Integer

PLS.T2

331

PLS.T3

332

PLS.T4

333

PLS.T5

334

PLS.T6

335

PLS.T7

336

PLS.T8

337

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

658

PLS.T1

No 16 bit No

M_01-03-00-000

660

PLS.T2

662

PLS.T3

664

PLS.T4

666

PLS.T5

668

PLS.T6

670

PLS.T7

672

PLS.T8

Related Topics

Programmierbarer Endschalter