PLS.WIDTH1 TO PLS.WIDTH8

Description

These parameter define the width of the PLS pulse for position-based PLS handling. For further information about the PLS functionality, especially the meaning of the PLS.WIDTH1 to PLS.WIDTH8 parameter, refer to the PLS.UNITS parameter.

General Information

Type

R/W parameter

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR

Range

N/A

Default Value

0

Data Type

Float

BASIC: Integer

See Also

PLS.EN, PLS.RESET, PLS.STATE, PLS.UNITS, PLS.MODE, PLS.P1 TO PLS.P8, PLS.T1 TO PLS T8

Start Version

M_01-02-03-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

34A1h/1

PLS.WIDTH1

M_01-02-03-000

34A1h/2

PLS.WIDTH2

34A1h/3

PLS.WIDTH3

34A1h/4

PLS.WIDTH4

34A1h/5

PLS.WIDTH5

34A1h/6

PLS.WIDTH6

34A1h/7

PLS.WIDTH7

34A1h/8

PLS.WIDTH8

Paramter

Fieldbus

Address

Attributes Signed?
PLS.WIDTH1

Profinet

2338 DWord Yes
sercos® III 8 Octets
PLS.WIDTH2

Profinet

2340 DWord
sercos® III 8 Octets
PLS.WIDTH3

Profinet

2342 DWord
sercos® III 8 Octets
PLS.WIDTH4

Profinet

2344 DWord
sercos® III 8 Octets
PLS.WIDTH5

Profinet

2346 DWord
sercos® III 8 Octets
PLS.WIDTH6

Profinet

2348 DWord
sercos® III 8 Octets
PLS.WIDTH7

Profinet

2350 DWord
sercos® III 8 Octets
PLS.WIDTH8

Profinet

2352 DWord
sercos® III 8 Octets

Fieldbus

Parameter

Instance

Data Size Data Type

EtherNet/IP

PLS.WIDTH1

339 8 Byte Signed Position

PLS.WIDTH2

341

PLS.WIDTH3

343

PLS.WIDTH4

345

PLS.WIDTH5

347

PLS.WIDTH6

349

PLS.WIDTH7

351

PLS.WIDTH8

353

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

676

PLS.WIDTH1

Yes 64 bit Yes

M_01-03-00-000

680

PLS.WIDTH2

684

PLS.WIDTH3

688

PLS.WIDTH4

692

PLS.WIDTH5

696

PLS.WIDTH6

700

PLS.WIDTH7

704

PLS.WIDTH8

Related Topics

Programmierbarer Endschalter