SD.STATUS
Description
This parameter reads the status of the SD card.
| Status | Description |
|---|---|
| 0 | Ready – an SD card is inserted into the drive and you can read and write to it. |
| 1 | Read Only – an SD card is inserted into the drive and the write protection tab on the card prohibits writes. |
| 2 | Not Inserted – an SD card is not inserted into the drive. |
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-06-03-000 |
Variants Supported
Supported by any AKD with an SD Card slot.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1688 |
No | 8-bit | No |
M_01-06-03-000 |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics