STRINGx.DRIVESIPADDRESS

Description

STRINGx.DRIVESIPADDRESS displays the IP addresses of all devices connected on string x.

When used without an index number it will return a list containing the IP addresses of all devices on the string.

When used with an index number it will display the IP address of a specific device instead, e.g. STRING1.DRIVESIPADDRESS 3 //displays the IP address of the 3rd device on the first string.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-16-02-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Die AKD-C zentrale Spannungsversorgung | STRINGx.NODECOUNT