STRINGx.DRIVESISFAULTED
Description
STRINGx.DRIVESISFAULTED displays the fault status of the drives connected to the AKD-C on string x. Each bit represents the fault status of one drive, starting with the fault status of the first drive in the least significant bit.
- 0 – drive has no faults
- 1 – drive has faults
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
0 to 255 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-17-01-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | No |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No |
| AKD EtherNet/IP | No |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | No |
| AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics