STRINGx.DRIVESMODEL
Description
STRINGx.DRIVESMODEL displays the model information for all devices connected on string x.
When used without an index number it will return a list containing the model information for all devices on the string.
When used with an index number it will display the model information of a specific device instead.
STRING1.DRIVESMODEL 3 //displays the model information of the 3rd device on the first string.
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-16-01-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | No |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No |
| AKD EtherNet/IP | No |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | No |
| AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics