STRINGx.DRIVESSTOSTATE

Description

STRINGx.DRIVESSTOTYPE displays the STO type of the drives connected to the AKD-C on string x. Each bit represents the STO type of one drive, starting with the STO type of the first drive in the least significant bit.

  • 0 – remote STO
  • 1 – local STO

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 255

Default Value

N/A

Data Type

Integer

Start Version

M_01-16-01-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Die AKD-C zentrale Spannungsversorgung | STRINGx.DRIVESSTOSTATE