STRINGS.IPMODERESET

Description

If the AKD-N’s connected to the AKD-C are set to an invalid static ip address, the command STRINGS.IPMODERESET on the AKD-C can be used to reset the ip mode of all AKD-Ns. After execution of this command, the AKD-N retrieve a new IP address either through DHCP or Auto IP.


  • This command will only effect AKD-N’s with FW version greater or equal to M_01-14-00-003.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-14-00-003

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Die AKD-C zentrale Spannungsversorgung