STRINGS.PHASELOSSFTHRESH

Description

When a phase loss is detected, a fault (F451, F452, or F453) is triggered only if the string current is larger than the value of STRINGS.PHASELOSSFTHRESH. Otherwise a warning is displayed.

General Information

Type

R/W Parameter

Units

Arms

Range

0 to DRV.IPEAK

Default Value

8 Arms

Data Type

Float

Start Version

M_01-13-11-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Die AKD-C zentrale Spannungsversorgung