STRINGS.STOSTATEMASK

Description

STRINGS.STOSTATEMASK reads which strings have drives with remote STO connected. Each bit represents one string, starting with string 1 in the least significant bit.

Value Description
0 No drives with remote STO connected
1 At least one drive with remote STO connected

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 255

Default Value

N/A

Data Type

Integer

Start Version

M_01-016-04-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC No
AKD SynqNet No
AKD EtherNet/IP No
AKD Profinet No
AKD sercos® III No
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Die AKD-C zentrale Spannungsversorgung