TEMP.CONTROL

Description

Reads the temperature of the control board temperature sensor.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-127 to 128

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2874

Word Yes
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 875 2 Byte Signed Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

1748

No 16-bit Yes

Related Topics

DRV.TEMPERATURES | TEMP.POWER1 to TEMP.POWER3