VBUS.PHASESTATE
Description
VBUS.PHASESTATE displays which input phases are connected to the device. Each bit represents one phase, starting with phase 1 in the least significant bit. The bit is set when the phase is connected.
Example
Only phases 1 and 2 are connected. VBUS.PHASESTATE will read 3 (binary 011).
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
0 to 7 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-18-02-000 |
Variants Supported
| Variant | Supported |
|---|---|
| AKD Base | No |
| AKD with Position Indexer | No |
| AKD EtherCAT | No |
| AKD CANopen | No |
| AKD BASIC | No |
| AKD SynqNet | No |
| AKD EtherNet/IP | No |
| AKD Profinet | No |
| AKD sercos® III | No |
| AKD-N | No |
| AKD-C | Yes |
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
3088 |
No | 8-bits | No |
M_01-18-02-000 |