VL.FBDISPLAYCUTOFF

Description

The parameter VL.FBDISPLAYCUTOFF defines the cutoff frequency for the filtered signal VL.FBDISPLAY.

With default value to 0, the raw velocity signal is unfiltered.

General Information

Type

N/V Parameter

Units

Hz

Range

0 to 2000

Default Value

0

Data Type

Float

See Also

VL.FBDISPLAY

Start Version

M_01-19-02-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

N/A

N/A

Fieldbus

Address

Attributes Signed?

Profinet

2428

DWord Yes
sercos® III 8 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 1158 4 Byte Signed Velocity

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

3130

No 32 Bit No

M_01-19-02-000