WS.DISARM

Description

This command disables wake and shake immediately. Feedback type is not relevant for this command. If WS.ARM has been issued, the request to execute the wake and shake algorithm at the next enable is cancelled. WS.STATE is set to IDLE.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Start Version

M_01-04-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Address

Attributes Signed?

Profinet

2847

Command* No
sercos® III

 

Fieldbus Instance Data Size Data Type
EtherNet/IP 848 Command None

*For Profinet, write a value of 0 into the PNU to execute a command.

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1694

No Command No

M_01-06-03-000

Related Topics

Wake and Shake Übersicht