WS.TSTANDSTILL

Description

In Wake & Shake mode 1, a maximum current of WS.IMAX is applied to the motor. WS.TSTANDSTILL defines a wait time, during which this maximum current is held, before detecting the commutation angle of the motor. Longer times are useful for big inertia motors or heavy loads.

General Information

Type

R/W Parameter

Units

ms

Range

100 to 20,000

Default Value

1000

Data Type

U16

Start Version

M_01-06-07-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

535Ch /0

M_01-06-07-000

Fieldbus

Address

Attributes Signed?

Profinet

2860

Word No
sercos® III 2 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 861 2 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Modbus

1720

No 16-bit No

Related Topics

Wake and Shake Übersicht | WS.MODE | WS.TIRAMP