ACTION#.ERROR

Description

ACTION#.ERROR returns the latest error during execution of an action task.

The information returned includes:

  • A timestamp. What DRV.RUNTIME was when the error happened.
  • A keyword name, if the error was related to execution of a keyword
  • An error code and a description of the cause of the error

Clearing faults or warnings on either axis or for the whole drive will clear all errors. Deactivating or successfully executing an action will clear that action’s error.

Examples

Action 7 is configured for starting a motion task. When it is triggered while the drive is disabled ACTION.ERRORS will return the following output:

-->ACTION7.ERROR
03d:14h:28m:29s:021ms:689us, AXIS1.MT.MOVE, [0012] Axis disabled! Enable axis first.

Versions

Action Version Notes
Implemented 02-09-01-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.