AXIS#.FBUS.ACC

Description

This command allows reading the acceleration set by fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile position, Profile velocity
CAN Profile position, Profile velocity
PROFINET MDI_ACC signal, accel limit used when commanding velocity
EtherNet/IP Accel limit used for command types 6 (position move) and 7 (jog)

  • Writing to this command is possible and is used when AXIS#.CMDSOURCE is fieldbus. Depending on the fieldbus mode, may be overwritten by the fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2

See Acceleration Units.

Range

Depends on units. See Acceleration Units.

Default Value

10,000 RPM/s

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.FBUS.ACC

5100

13EC

Unsigned32

Read/Write

Acceleration

AXIS2.FBUS.ACC

70636

113E

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.ACC

5100

Float

Read/Write

Acceleration