AXIS#.IL.FOLDWTHRESH
Description
AXIS#.IL.FOLDWTHRESH is the warning level of the current foldback algorithm. When AXIS#.IL.IFOLD drops below AXIS#.IL.FOLDWTHRESH and foldback is active, a warning is generated.
To ensure that the current foldback warning level is never reached, AXIS#.IL.FOLDWTHRESH should be set well below the continuous current value for both the drive and motor, namely AXIS#.ICONT and AXIS#.MOTOR.ICONT respectively. You can also set the AXIS#.IL.FOLDWTHRESH value to zero.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Arms |
Range |
0 to 500 Arms |
Default Value |
Drive_IPEAK |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.IL.FOLDWTHRESH |
500ah |
0ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.IL.FOLDWTHRESH |
510ah |
0ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.IL.FOLDWTHRESH |
5807 |
16AF |
Signed32 |
Read/Write |
- |
AXIS2.IL.FOLDWTHRESH |
71343 |
116A |
Signed32 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.FOLDWTHRESH |
5807 |
Float |
Read/Write |
- |