AXIS#.JOG.ACC

Description

This keyword sets the acceleration ramp for jog moves.

Versions

Action Version Notes
Implemented 02-04-01-000  

General Information

Type Read/Write
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2

See Acceleration Units for details.

Range Depends on units. See Acceleration Units for details.
Default Value

30,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.JOG.ACC

501bh

01h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.JOG.ACC

511bh

01h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.JOG.ACC

6900

1AF4

Unsigned32

Read/Write

Acceleration

AXIS2.JOG.ACC

72436

11AF

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.JOG.ACC

6900

Float

Read/Write

Acceleration