AXIS#.PL.CMD

Description

AXIS#.PL.CMD reads the position command as it is received in the position loop entry.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units Rotary: counts, rad, deg, custom units, 16-bit counts. See Position Units for details.
Range Depends on units. See Position Range for details.
Default Value N/A
Data Type Float
See Also AXIS#.PL.FB
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.CMD

6062h

00h

Signed32

Position

-

Read only

Yes

AXIS2.PL.CMD

6862h

00h

Signed32

Position

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.CMD

5900

170C

Signed32

Read Only

Position

AXIS2.PL.CMD

71436

1170

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.CMD

5900

Signed32

Read Only

Position

Related Topics

AXIS#.PL.ERR | AXIS#.PL.ERRFTHRESH | AXIS#.PL.ERRWTHRESH |

Position Loop