MW.MODEL#.STATE

This command allows you to specify which MechaWare models run. There is a command for each model loaded on the drive. The value of the command specifies whether the model runs (1) or is disabled (0).

Models 1-4 are Factory Models loaded by Kollmorgen. Models 5-8 are User Models.

Example

Enable Model 1:

-->MW.MODEL1.STATE 1

Get the excitation current (already set to 0.2 A):

-->MW.MODEL1.STATE
1

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write
Description Sets the operating state of the Kollmorgen Automation Suite model
Units N/A
Range 0-1
Default Value 1
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MW.MODEL1.STATE

30e3h

01h

Unsigned8

-

-

Read/Write

No

MW.MODEL2.STATE

30e3h

02h

Unsigned8

-

-

Read/Write

No

MW.MODEL3.STATE

30e3h

03h

Unsigned8

-

-

Read/Write

No

MW.MODEL4.STATE

30e3h

04h

Unsigned8

-

-

Read/Write

No

MW.MODEL5.STATE

30e3h

05h

Unsigned8

-

-

Read/Write

No

MW.MODEL6.STATE

30e3h

06h

Unsigned8

-

-

Read/Write

No

MW.MODEL7.STATE

30e3h

07h

Unsigned8

-

-

Read/Write

No

MW.MODEL8.STATE

30e3h

08h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

MW.MODEL1.STATE

2801

AF1

Unsigned8

Read/Write

-

MW.MODEL2.STATE

2802

AF2

Unsigned8

Read/Write

-

MW.MODEL3.STATE

2803

AF3

Unsigned8

Read/Write

-

MW.MODEL4.STATE

2804

AF4

Unsigned8

Read/Write

-

MW.MODEL5.STATE

2805

AF5

Unsigned8

Read/Write

-

MW.MODEL6.STATE

2806

AF6

Unsigned8

Read/Write

-

MW.MODEL7.STATE

2807

AF7

Unsigned8

Read/Write

-

MW.MODEL8.STATE

2808

AF8

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

MW.MODEL1.STATE

2801

Unsigned8

Read/Write

-

MW.MODEL2.STATE

2802

Unsigned8

Read/Write

-

MW.MODEL3.STATE

2803

Unsigned8

Read/Write

-

MW.MODEL4.STATE

2804

Unsigned8

Read/Write

-

MW.MODEL5.STATE

2805

Unsigned8

Read/Write

-

MW.MODEL6.STATE

2806

Unsigned8

Read/Write

-

MW.MODEL7.STATE

2807

Unsigned8

Read/Write

-

MW.MODEL8.STATE

2808

Unsigned8

Read/Write

-