Copyrights, Trademarks, Patents, and Disclaimers
Copyright © 2026 Regal Rexnord Corporation, All Rights Reserved.
Information in this document is subject to change without notice. The software package described in this document is furnished under a license agreement. The software package may be used or copied only in accordance with the terms of the license agreement.
This document is the intellectual property of Kollmorgen and contains proprietary and confidential information. The reproduction, modification, translation or disclosure to third parties of this document (in whole or in part) is strictly prohibited without the prior written permission of Kollmorgen.
Kollmorgen Trademarks
Regal Rexnord and Kollmorgen are trademarks of Regal Rexnord Corporation or one of its affiliated companies.
These trademarks or tradenames are owned by or under the control of Regal Rexnord Corporation or any of its affiliates:
- SafeMotion
- SMM
Other Trademarks
These trademarks or tradenames are not owned by or under the control of Regal Rexnord Corporation or any of its affiliates:
- EnDat, Dr. Johannes Heidenhain GmbH.
- EtherCAT, Beckhoff Automation GmbH.
- EtherCAT and Safety over EtherCAT, Beckhoff Automation GmbH, Germany.
- EtherNet/IP, ODVA, Inc.
- HIPERFACE, Max Stegmann GmbH.
- Modbus, Schneider Electric USA, Inc.
- PROFINET, PROFIBUS Nutzerorganisation e.V.
- Windows, Microsoft Corporation.
Patents
Current patents
- US Patent 2017/0211640 (method and apparatus for power saving, fail-safe control of an electromechanical brake), patent pending
- US Patent 16,247,478 (method and apparatus for limiting the output voltages of switching mode power supplies), patent pending
- US Patent 8,154,228 (Dynamic Braking For Electric Motors)
- US Patent 8,214,063 (Auto-tune of a Control System Based on Frequency Response)
- US Patent 10,374,468 (System and method for improved DC power line communication)
Patents referring to fieldbus functions are listed in the matching fieldbus manual.
Disclaimers
Technical changes which improve the performance of the device may be made without prior notice!
This document is the intellectual property of
The information in this document is believed to be accurate and reliable at the time of its release. Kollmorgen assumes no responsibility for any damage or loss resulting from the use of this help, and expressly disclaims any liability or damages for loss of data, loss of use, and property damage of any kind, direct, incidental or consequential, in regard to or arising out of the performance or form of the materials presented herein or in any software programs that accompany this document.
Technische Änderungen, die der Verbesserung der Geräte dienen, vorbehalten!
Dieses Dokument ist geistiges Eigentum von
Die Genauigkeit und Verlässlichkeit der Informationen in diesem Dokument entspricht dem Kenntnisstand zum Zeitpunkt der Veröffentlichung. Kollmorgen übernimmt keine Verantwortung für Schäden oder Verluste, die sich aus der Verwendung dieser Hilfe ergeben, und lehnt ausdrücklich jegliche Haftung sowie Schadensersatzansprüche für Datenverlust, entgangene Nutzung und Sachschäden jeglicher Art ab, inklusive direkter, zufälliger oder Folgeschäden im Zusammenhang mit der Funktion oder Form des hierin oder in einem der mit diesem Dokument gelieferten Software enthaltenen Materials.
Es posible que se implementen sin aviso previo cambios técnicos que mejoran el rendimiento del dispositivo.
La propiedad intelectual de este documento pertenece a
La información incluida en este documento se considera correcta y confiable en el momento de su publicación. Kollmorgen no asume ninguna responsabilidad por ningún daño o pérdida causados por el uso de este documento de ayuda y rechaza explícitamente toda responsabilidad o daño por pérdida de datos, pérdida de uso y daños en la propiedad de cualquier tipo, ya sea directos, incidentales o consecuentes, en relación con el rendimiento o la forma de los materiales aquí publicados, o con los programas de software que acompañan a este documento, o que surjan de estos.
Les modifications techniques qui améliorent les performances du dispositif peuvent être apportées sans avis préalable !
Ce document est la propriété intellectuelle de
Les informations contenues dans ce document sont considérées exactes et fiables au moment de leur publication. Kollmorgen n'assume aucune responsabilité pour tout dommage ou perte résultant de l'utilisation de cette aide, et rejette expressément toute responsabilité ou tous dommages pour la perte de données, la perte d'utilisation et les dommages matériels de toute nature, directs, accessoires ou indirects, en ce qui concerne ou découlant des performances ou de la forme des matériaux présentés ici ou dans tout programme logiciel accompagnant ce document.
Modifiche tecniche volte a migliorare le prestazioni del dispositivo possono essere apportate senza preavviso.
Il presente documento è proprietà intellettuale di
Le informazioni contenute nel presente documento sono ritenute accurate e affidabili al momento della pubblicazione. Kollmorgen non si assume alcuna responsabilità per eventuali danni o perdite risultanti dall'uso di questa guida e declina espressamente qualsiasi responsabilità o danni dovuti a perdita di dati, mancato utilizzo e danni materiali di qualunque tipo, diretti, accidentali o consequenziali, in relazione a o derivanti dal funzionamento o dalla forma dei materiali presentati qui o in eventuali programmi software che accompagnano il presente documento.
Alterações técnicas que melhoram o desempenho do dispositivo podem ser feitas sem aviso prévio!
Este documento é propriedade intelectual da
Acredita-se que as informações contidas neste documento sejam precisas e confiáveis no momento de sua divulgação. A Kollmorgen não assume nenhuma responsabilidade por quaisquer danos ou perdas resultantes do uso desta ajuda, e se isenta expressamente de qualquer responsabilidade ou danos por perda de dados, perda de uso e danos materiais de qualquer espécie, direta, incidental ou subsequente em relação a ou resultante do desempenho ou da forma dos materiais apresentados aqui ou em quaisquer programas de software que acompanhem este documento.
我们可能会进行技术更改以提高设备性能,恕不另行通知!
本文档知识产权归
据我们所知,本文档所含信息截至发布日是准确可靠的。对于因使用本帮助文档而导致的任何损害或损失,Kollmorgen概不承担任何责任。Kollmorgen特此明确声明,对于因本文档中的任何材料或随附本文档之任何软件程序的性能或形式导致的或与之相关的任何类型的数据丢失、使用中断损失或财产损害(包括直接、间接和衍生性损失或损害),Kollmorgen不承担任何法律责任或损害赔偿责任。