AXIS#.CANOPEN.GEARPRIMARY.SHAFTREV
Description
This keyword provides the count of driving shaft revolutions for the primary position gear ratio calculation. It is part of the scaling calculation used for CANopen objects.
Context
See CANopen Scaling.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
1 to 4294967295 |
Default Value |
1 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
CAN bus and EtherCAT
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.CANOPEN.GEARPRIMARY.SHAFTREV |
6091h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |
AXIS2.CANOPEN.GEARPRIMARY.SHAFTREV |
6891h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |