AXIS#.MOTOR​.FIELDWEAKENING

Description

This parameter turns on field weakening control for rotary surface permanent magnet and interior permanent magnet motors (AXIS#.MOTOR.TYPE = 0 and 6). Field weakening allows a motor to operate above rated speed.

This keyword can only be set when AXIS#.MOTOR.TYPE = 0, 6, or 10. Any other AXIS#.MOTOR.TYPE results in an error and AXIS#.MOTOR.FIELDWEAKENING is not applied.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.FIELDWEAKENING

500bh

0fh

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.FIELDWEAKENING

510bh

0fh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6236

1

6236 (0x185c)

AXIS1.MOTOR.FIELDWEAKENING

Unsigned8

Read/Write

Yes

71772

2

6236 (0x185c)

AXIS2.MOTOR.FIELDWEAKENING

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.FIELDWEAKENING

6236

Unsigned8

Read/Write

-