AXIS#.MT.TYPE

Description

This keyword sets the motion task control word with the motion task type information.

It takes the following values:

0 Absolute
1 Relative To Command Position
2 Relative to previous target position
3 Relative to external position
4 Relative to feedback position

Examples

Usage

This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.

Code

MT.TYPE 0 2 Will configure Motion Task 0 as a move relative to previous target position.

Context

See AXIS#.MT.CNTL for more information on the argument semantics.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only Array
Units N/A
Range 0 to 4
Default Value 0
Data Type Integer
See Also  
Start Version  

Stored in Non-Volatile Memory

No

Variants Supported

Supported on all drives.

Fieldbus Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6318

1

6318 (0x18ae)

AXIS1.MT.TYPE

Unsigned8[32]

Read/Write

Yes

71854

2

6318 (0x18ae)

AXIS2.MT.TYPE

Unsigned8[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.TYPE

6318

Unsigned8[32]

Read/Write

-