AXIS#.PROFINET.MAXSOLFAIL
Description
The maximum number of times the sign of life value can be incorrect before faulting. This is used when IRT is active on the PROFINET network to ensure synchronization is maintained.
When set to 65535 the sign-of-life fault detection is disabled.
See Controlword/Statusword 2 and Sign of Life (STW2/ZSW2).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-02-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | 0-65535 |
| Default Value | 1 |
| Data Type | Integer |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Industrial Ethernet Information
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.PROFINET.MAXSOLFAIL |
925 |
Unsigned16 |
Read/Write |
- |