AXIS#.SENSORLESS.RPMSTART
Description
Sensorless Field-Oriented Control (SFOC) runs in open-loop when velocity is below a certain limit and automatically switches to closed loop when velocity goes above that limit. This limit is determined by AXIS#.SENSORLESS.RPMSTART. There is a hysteresis band to make the transition seamless.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-03-03-000 |
|
General Information
Type |
Read/Write |
Description | Sets the starting velocity for SFOC |
Units |
rpm |
Range |
0 to Maximum Motor Velocity |
Default Value |
300 |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SENSORLESS.RPMSTART |
5018h |
06h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
AXIS2.SENSORLESS.RPMSTART |
5118h |
06h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.SENSORLESS.RPMSTART |
7404 |
1CEC |
Signed32 |
Read/Write |
- |
AXIS2.SENSORLESS.RPMSTART |
72940 |
11CE |
Signed32 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.SENSORLESS.RPMSTART |
7404 |
Float |
Read/Write |
- |