AXIS#.SWLS.EN
Description
This parameter enables the software travel limit switches.
-
- The software limit switches are only active if the axis is homed.
Examples
Usage
0: Disable both software limit switches
1: Enable software limit switch 0, AXIS#.SWLS.LIMIT0
2: Enable software limit switch 1, AXIS#.SWLS.LIMIT1
3: Enable both software limit switches
If AXIS#.SWLS.EN = 3, then whichever limit switch is set to a greater value will be used as the upper limit switch. For all other values of AXIS#.SWLS.EN, use AXIS#.SWLS.LIMIT0 for the lower limit switch and AXIS#.SWLS.LIMIT1 for the upper limit switch.
"AXIS#.CS.DEC " is executed when a SWLS is triggered. The user can set the CS.DEC value, or go with the default 10,000 rpm/s. Once the switch is triggered, a warning W6006 results, and the position/load must be moved back within the limits to remove the warning.
Code
Axis 1 lower limit switch set to 1000 and upper limit switch set to 5000. Axis 1 home position is set and then both software limit switches are enabled.
-->AXIS1.SWLS.LIMIT0 1000 -->AXIS1.SWLS.LIMIT1 5000 -->AXIS1.HOME.SET -->AXIS1.SWLS.EN 3
Context
For more information on limit switches, refer to Limits.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 3 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | AXIS#.SWLS.STATE, AXIS#.SWLS.LIMIT0, AXIS#.SWLS.LIMIT1 |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SWLS.EN |
500fh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.SWLS.EN |
510fh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6500 |
1 |
6500 (0x1964) |
AXIS1.SWLS.EN |
Unsigned8 |
Read/Write |
Yes |
|
72036 |
2 |
6500 (0x1964) |
AXIS2.SWLS.EN |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.SWLS.EN |
6500 |
Unsigned8 |
Read/Write |
- |