AXIS#.FAULTS
Description
Indicates what faults are present on an axis.
Examples
In a scenario where two faults are present on Axis 1 (faults 4312 and 4115), the following output would be seen:
-->AXIS1.FAULTS
4312: Feedback: Broken Wire fault.
4115: Failed to set feedback type.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | N/A |
Range | N/A |
Default Value | N/A |
Data Type | String |
See Also | DRV.FAULTS |
Stored in Non-Volatile Memory |
No |
Variants Supported
Supported on all device types.