AXIS#.SAFEPARAM.SOS_x.SAFEINPUT
Description
Indicates which safe input triggers the Safe Operating Stop (SOS) safety function.
| Value | Description |
|---|---|
|
0 |
Not used |
|
1 |
Safe Input 1 (SIN1) |
|
2 |
Safe Input 2 (SIN2) |
|
3 |
Safe Input 3 (SIN3) |
|
4 |
Safe Input 4 (SIN4) |
|
5 |
Safe dual input 1 (SIN1/SIN2) |
|
6 |
Safe dual input 2 (SIN3/SIN4) |
Context
For complete SOS information refer to SOS (Safe Operating Stop).
Related safety parameters:
- AXIS#.SAFE.SOS_x.INTERNALSTATE
- AXIS#.SAFEPARAM.SOS_x.FSOE
- AXIS#.SAFEPARAM.SOS_x.FUNCTIONACTIVATION
- AXIS#.SAFEPARAM.SOS_x.POSZEROWINDOW
- AXIS#.SAFEPARAM.SOS_x.RESTARTACKBEHAVIOR
- AXIS#.SAFEPARAM.SOS_x.RESTARTACKSOURCE
- AXIS#.SAFEPARAM.SOS_x.TIMEDELAYMONITORING
- AXIS#.SAFEPARAM.SOS_x.VELZEROWINDOW
- AXIS#.SAFEPARAM.SOS_x.VELMONITOREN
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.54 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1, 2, 3, 4, 5, 6 |
|
Default Value |
0 (Not used) |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.SAFEPARAM.SOS_1.SAFEINPUT |
315bh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS1.SAFEPARAM.SOS_2.SAFEINPUT |
3172h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.SOS_1.SAFEINPUT |
325bh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
AXIS2.SAFEPARAM.SOS_2.SAFEINPUT |
3272h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |