Post Processing Smoothing %
The Smoothing % parameter can help the automatic tuner make better use of a low resolution or noisy encoder.
-
-
Important Notes about using Smoothing
-
Increasing the Smoothing too much will smooth out resonant peaks, making them look not as severe as they really are.
-
Only use smoothing when increasing the excitation amplitude doesn’t work. You need accurate data before you start processing the data
-
Post Processing Smoothing Example
The plot has poor quality data because a low excitation was used. In this measurement the Smoothing % is 1.000. Note that the resonant peak shows up as +5.1 dB

In the following image the smoothing has been increased to 4.000% rather than increasing the amplitude. Now, we have what appears to be clean data, but how accurate is it? The resonant peak dropped from +5.1 dB to -6 dB.
The difference in the resonant peak values is ~ 11dB, which is almost twice what is normally allocated for gain margin.
-
-
Always increase Amplitude before increasing Smoothing.