AXIS#.CANOPEN​.FB#.DIR

Description

This parameter can be used to reverse the direction for the associated additional feedback position (60E4h) when using EtherCAT or CANopen.


  • This does not affect the position displayed in WorkBench or the position used by an axis. It is intended for when a feedback is used as an external encoder by a PLC separate from a specific axis. To change the axis’ direction, use AXIS#.DIR.

Value

Description

0 (Default)

Normal direction. Encoder positions increment in the direction as given by the feedback device.

1

Inverted direction. The position from the encoder is inverted and will count in the opposite direction as given from the feedback device.

Versions

Action Version Notes
Implemented 02-08-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 – Normal direction

1 – Inverted direction

Default Value

0 – Normal Direction

Data Type

Unsigned8

See Also

60E4h

Stored in Non-Volatile Memory

Yes

Variants Supported

AKD2G-SPE (EtherCAT)

AKD2G-SPC (CANopen)

KED-SPM (Multi-Ethernet)

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.CANOPEN.FB1.DIR

60f1h

01h

Unsigned8

-

-

Read/Write

No

AXIS1.CANOPEN.FB2.DIR

60f1h

02h

Unsigned8

-

-

Read/Write

No